AXIS#.CANOPEN.FCPRIMARY.FEED
Description
This keyword provides the feed for the primary position feed constant calculation. It is part of the scaling calculation used for CANopen objects.
Context
See CANopen Scaling.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 4294967295 |
|
Default Value |
65536 (2^16) |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
CAN bus and EtherCAT
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.CANOPEN.FCPRIMARY.FEED |
6092h |
01h |
Unsigned32 |
- |
- |
Read/Write |
No |